This Guide was developed to convey the primary changes to the 2014 NEC when compared to the 2011 NEC. This enables electrical and low-voltage professionals to keep informed and stay in Code compliance from one Code cycle to the next. Articles covered primarily relate to Wiring Devices and Communications Systems with limited discussion of Over-Current Protection, Raceways, Wires, Luminaries, Emerging Markets and other mainstream requirements.
Note: Leviton Manufacturing Company assumes no responsibility for interpretation or application of this publication and its contents.
Text Legend | |
Category | Color Style |
Summary of Change | Standard black text |
Actual NEC text from NFPA 70 | Serif-style font within green box |
Expert Analysis | Standard black text |
New NEC text for 2014 | Shaded serif-style font within green box |
Previous 2017 NEC® Text Removed for 2020 | |
Leviton commentary | Insights from Leviton Manufacturing are in green text |
Leviton Solutions | Leviton solutions which address applicable code articles are in blue text |
Material taken from the National Electrical Code® is reprinted with permission from NFPA 70® - 2020 edition, National Electrical Code®, Copyright 2019, National Fire Protection Association®, Quincy, MA. All rights reserved. This material is not the complete and official position of the NFPA on the reference subject, which is represented only by the standard in its entirety a copy of which can be obtained through the NFPA web site at www.nfpa.org.
National Electrical Code®, NEC® and NFPA 70® are registered trademarks of the
National Fire Protection Association®, 1 Batterymarch Park, Quincy, MA 02169
The National Fire Protection Association did not produce, review or approve this book and assumes no responsibility for the application or use of any NEC® related material set out herein.
Leviton, the Leviton logo, Decora®, Decora Smart™, SmartlockPro®, Wetguard®, Opt-X®,
e2HXD®, and Lightspace® are trademarks of Leviton Manufacturing Co., Inc.